简介
With the Simplicity Studio 5 (SSv5) 5.6.0.0 release, Silicon Labs introduced support for using Visual Studio Code (VS Code) in combination with Simplicity Studio. At its core, this extension enables building, flashing, and debugging from within the VS Code Ecosystem. While still allowing use of the project configuration GUIs that you know and love from with Simplicity Studio itself.
To enable the support mentioned above, a VS Code extension is required. It can be installed directly from within Visual Studio Code, or downloaded to disk in the marketplace. The preferred method of installation is to install it from the marketplace within the VS Code application itself.
Simplicity Studio will still be used to create the initial project and target it for Visual Studio Code. This will enable all editing, building, and debugging of the project should be done in VS Code.
特点
Build, flash and debug compatible projects
Utilization of CMake and Ninja
Detect compatible projects from VS Code active workspace
Detect locally connected 32-bit Silicon Lab devices
Detect remotely connected 32-bit Silicon Lab devices
下载
In order to obtain the extension you can download it at the link below. However, the prefered method of installation is to utilize the extensions browser from within Visual Studio Code and search for "Simplicity Studio for VS Code" and install directly in the application.
技术文档
社区与支持
知识库文章
浏览我们的知识库文章,了解特定产品信息。
用户论坛
浏览技术问题,分享您的想法,同时进一步了解我们的最新解决方案。
Visual Studio Marketplace Forum
Browse questions and responses from the visual studio marketplace.
问题?您来对了地方。
Silicon Labs 拥有由工程师和开发人员组成的用户社区,该社区活跃度高、成员知识丰富,热衷于解决问题。