简介
Simplicity Commander is a utility that provides GUI and command line access to the debug features of an EFM32 device. It allows you to flash firmware, update the kit firmware, and lock, or unlock debug access. Commander can be accessed by either launching it form within Simplicity Studio, or by downloading the standalone version. Simplicity commander is available for the following operating systems:
- Windows x64
- Mac OS X
- Linux x86, ARM32, ARM64
You can find download for each on the download portion of this page.
特点
对设备上的闪存内容进行编程、擦除和读取
使用 CLI,根据需要编写命令脚本
读、写、解析令牌或 NVM3 内容
配置和升级硬件套件固件
通过对固件图像、锁定调试访问和其他选项执行签名和加密操作,确保设备安全
下载
技术文档
社区与支持