简介
Simplicity Studio® 5 (SSv5)'s Network Analyzer enables debugging of complex wireless systems. This tool captures a trace of wireless network activity that can be examined in detail live or at a later time.
More than simply a packet sniffer, the Network Analyzer works with the data sniffer interface on the Silicon Labs wireless chips to provide direct feedback from the baseband radio of each device, allowing any supported radio to report detailed packet transmission and reception data, such as timestamps, link quality (or LQI), receive sensitivity (or RSSI), and CRC pass/fail results, all without any software overhead.
With SSv5, any PTI-enabled Silicon Labs platform can record the radio activity regardless of the application firmware that is being used, so there’s no need to have a dedicated sniffer device installed to catch the traffic. The Network Analyzer also enables capture from multiple sources simultaneously into the same log file without falsely duplicating packets. This enables the developer to compare how well different radios in the network heard the same transmission.
特点
分析 EFR32 设备无线电发送或接收的数据
根据实施协议(例如,BLE、Zigbee、Z-Wave)对原始数据进行解码
将无线电活动可视化为单个数据包或事务(数据包组)
将多个来源的数据采集到同一日志文件中
下载
Network Analyzer is currently included with Simplicity Studio 5 as an integrated tool.
技术文档
社区与支持